header_contact_us

New DENSO VS-Series Aseptic Robot

New DENSO VS-Series Aseptic Robot

Sterilizable, for Pharmaceutical, Medical and Life Sciences Applications

LONG BEACH, Calif. — DENSO Robotics announced introduction of its new compact, high-speed, VS-050 six-axis aseptic robot, which features an ISO 5 cleanroom rating and specially designed coverings, for applications where biocontamination control is required..

“We created the VS-050 aseptic robot because of rapidly increasing demand in the pharmaceutical, medical and life sciences sectors,” said Peter Cavallo, robotics sales manager, DENSO Products & Services Americas, Inc. “Now our customers in those areas with sterilization requirements can benefit from the high speed and other outstanding features of the VS Series.”

A protective outer coating and sealed joints allow the VS-050 to be safely sterilized with hydrogen peroxide or UV light. The smooth, rounded exterior of the robot has no external screws, to keep dirt, dust or other contaminants from adhering to its surface. Wires are internally embedded up to the flange and the control-cable connector is located on the bottom of the robot, further streamlining the arm and facilitating cleaning.

DENSO’s VS-Series robots offer the world’s highest speed and precision in their class. The VS-050 aseptic model has a cycle time of 0.37 sec. and repeatability of ±0.02 mm, with a reach of 520 mm and a payload capacity of 4 kg.

Typical applications of the VS-050 include assembly, dispensing, inspection, machine tending, material handling, packaging and test handling.

For more information, visitwww.densorobotics.com/products/vs-050-060/data-sheet.

DENSO is the world’s largest user of small assembly robots, with more than 17,000 DENSO robots designed and used in its own manufacturing facilities. More than 77,000 additional DENSO robots are used by other companies worldwide.

DENSO robots are available with payloads up to 20 kg, reaches from 350 to 1,300 mm and repeatability to within ±0.015 mm. DENSO's compact, space-saving design facilitates integration, while a high maximum moment of inertia allows a wide variety of end effectors and applications. Standard (IP40), dust- and mistproof (IP65), dust- and splashproof (IP67), cleanroom (ISO 3, 4 and 5) and aseptic (H2O2-resistant) models are available. ANSI and CE compliance enables global deployment. UL-listed models are available for the U.S. and Canada. For more information,visit www.densorobotics.com.

DENSO Corporation, headquartered in Kariya, Aichi prefecture, Japan, is a leading global automotive supplier of advanced technology, systems and components in the areas of thermal, powertrain control, electronics and information and safety. Its customers include all the world's major carmakers. Worldwide, the company has more than 200 subsidiaries and affiliates in 38 countries and regions (including Japan) and employs nearly 140,000 people. Consolidated global sales for the fiscal year ending March 31, 2014, totaled US$39.8 billion. Last fiscal year, DENSO spent 9 percent of its global consolidated sales on research and development. DENSO common stock is traded on the Tokyo and Nagoya stock exchanges.

Currently, in North America, DENSO employs more than 17,000 people at 33 consolidated companies and affiliates. Of these, 28 are manufacturing facilities located in the U.S., Canada and Mexico. In the U.S. alone, DENSO employs more than 14,000 people in California, Alabama, Michigan, North Carolina, South Carolina, Tennessee, Kentucky, Georgia, Iowa, Ohio, Arkansas and Pennsylvania. DENSO’s North American consolidated sales totaled US$7.9 billion for the fiscal year ending March 31, 2014.

Back to News & Events